We are using LM3410 to control LED backlight brightness by using analog PWM with following circuit topology.
we are seeing failures with LM3410 (burned IC) under following two conditions
1- When C71 is installed the additional capacitance damages LM3410 with load present (LEDs are plugged in). When capacitance is set to 4.7uf (removing C71), the circuit works as intended.
2- With C71 removed, When following circuit is powered without any load (no LEDs plugged in) LM3410 is damaged.
Both failures require replacing LM3410.