Other Parts Discussed in Thread: GPCCHEM
I am having trouble getting the BQ40Z80 detecting a full charge.
I am charging a 6S 22.2V LiPo battery with a 1300mAh capacity. I set the design capacity settings (Design Capacity mAh = 1300mAh, Design Capacity cWh = 2886cWh, Design Voltage = 22200mV) The FC Set Voltage Threshold is set to 4200mV.
I set the ChemID and did the full discharge cycle as described by the Slua848 pdf and wait until the REST flag is set before starting the charge. I charge the battery all the way to 25.2V at a C/2 charge rate. The FC isnt set, and the battery is shown to only have a 31% charge. Remaining capacity is shown to be 1231mAh and Full charge Capacity is reported as 4097mAh.
What does the chip check to determine if the battery is at FC? Is it the voltage or is it comparing remaining charge to full charge capacity? Is there a setting I'm missing to configure?