This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3430: Resettable latching application

Part Number: TPS3430


Hello, We'd like to use TPS3430 in a latching application as per TI's published document SNVA837.  In summary, We're looking for WDO to stay asserted LOW upon the failure of DWI to reset the watchdog timer.

In addition we'd like to be able to reset the latched WDO output, restoring it to it's normal (disabled or active watchdog) operating conditions.  To accomplish this, we are thinking to connect the TPS3430 as follows:

VDD1/2 - 3.3V

WDI - GPIO input from NXP microprocessor

WDO - output with 10k pullup resistor

CWD - N/C

CRST - 5 nF capacitor to ground and open drain buffer from WDO

SET 0 - GPIO input from NXP microprocessor

SET 1 - 3.3V (HIGH)

The intended schematic is identical to what's provided in SNVA837 and also on p. 24 of the spec sheet for TPS3430 except for SET 0, which we're routing to a GPIO pin on an NXP micro.

Our understanding of this is as follows:

The TPS3430 can be powered up with SET 0 in either a high or low state successfully.  If SET 0 is HIGH upon power up, the device will remain disabled and WDO will remain HIGH until SET 0 is set LOW, at which point the watchdog timer will begin with tWDL ~ 22.5 ms and tWDU ~ 55 ms (with tolerance bands on these nominal values.)  If SET 0 is LOW upon power up, the watchdog timer will begin after a brief initialization.

If the window is ever missed, WDO will be asserted LOW (open drain), and remain latched LOW as long as the other pin states do not change.

If, from this WDO-asserted LOW (open drain) state, SET 0 is ever set HIGH, the device will be disabled entirely and WDO will be set back to HIGH. 

If, from the device's disabled state, SET 0 is set back to LOW, the watchdog timer will once again initialize with a 22.5 ms / 55 ms valid window.

Is this understanding correct?

Thanks!

Blake

  • Blake,

    I believe your understanding is correct, but I would like to take a closer look at the schematic. Do you have a capture of the actual schematic?

    Thanks,
    Abhinav.

  • Yes, we're still working on it, I'll provide it when it's finished.

    The detail that I'm least confident about is the resetting of the device.  On page 25 of the spec sheet for the TPS3430, the resetting of the watchdog counter as wired in that application is described as being possibly only by reducing VDD below VDD(min).  In the documented application, this makes sense, as both SET 0 and SET 1 are set high permanently.

    As mentioned in the first post, the only difference that will be evident for our application (as compared to the application mentioned in the spec sheet) is that SET 0 will be an input from a GPIO pin.  When we put SET 0 HIGH, will this disable the device and allow us to reset the timer?  This detail isn't completely clear to me.  From the triggered (WDO is LOW) state, we would put SET 0 HIGH briefly and then simultaneously set it LOW again while resuming pulses on WDI.

    Thanks and best regards,

    Blake

  • I also realized a slight mistake I made in the first post.  SET 1 is wired permanently LOW (so that when SET 0 is also LOW, the device is enabled, and when SET 0 is HIGH, the device is disabled.)

  • Hey Blake,

    I'm looking into this, but I was wondering if you had any updates in the meanwhile in terms of tests you did.

    Thanks,
    Abhinav.