This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5350: May I know what is the error in this circuit

Part Number: UCC5350


Hello,

 May I know  what would be mistake in this circuit.

Vp is a 5V pulse

Vcc2 is 15V, Vcc1 is 5V. 

If I give 15V pulse directly to the MOSFET, it is working fine. But if I connect the driver IC, simulation is not converging

Thanks for your kind response

Surya