This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: LM5146-Q1: VCC generation issue

Part Number: LM5146-Q1


HI,

we are designing a BUCK converter using LM5146Q1-  (Input range: 36Vdc to 72VDC  and Output : 12Vdc )

we have problem of generating VCC- 7.5V when we applied VIN in range of 36V to 72VDC and our UVLO pin voltage is greater than 1.2V.

VCC is not generated from input voltage 36V to 65V once input voltage  increase above 66V, it is generating 7.5V VCC.

we have not observed this issue in simulation.

Please look into this as we have stucked here.

Thanks and regards,

mahesh