Other Parts Discussed in Thread: TPS22916
In my circuit the Vout (1.2V for example) runs a plane to a device with several 1uF and 2.2uF capacitors on each pin (6 to be exact). I want the slowest rise time (> 100 usec) and the output continuous current is 120mA (est).The datasheet recommends a ratio of 10 to 1 (input capacitance to output capacitance. I estimate about 20 uF of capacitance required to supply and filter the device. I currently have a 10 uF capacitor on the output of my regulator a TPS62841. How do I determine what to put on the output of the load switch or is there a better device?
Thanks