Hi Team,
As for some automotive electronic product/application, they have requirement about passing iso 7637 5b
May I ask whether LMR33630-Q1 can meet the requirements of 7637 5b for these kinds of automotive electronic products?]
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
As for some automotive electronic product/application, they have requirement about passing iso 7637 5b
May I ask whether LMR33630-Q1 can meet the requirements of 7637 5b for these kinds of automotive electronic products?]
Thanks!
Hi,
LMR33630-Q1 could support the test if the Vin-GND pin voltage is kept below 38V for the transient. But on actual tests, it's better to use an input transient protection (typical TVS circuit) on the input in case any unexpected spikes on wire. Thanks.