Part Number: TPS2660
I have a question on reverse current blocking capability of TPS26601. When there's reverse current where Vin-Vout < -10mV, the internal FET will turns off after 1.5us and the ~FLT signal will be low after 45ms. Will the ~SHDN pin also goes low or remains high? Will the part turn on again after 70us when the differential voltage Vin-Vout > 96mV? I am asking this because I saw a reverse current after a current spike and the reverse current last for about 40us in my application and the part does not seem to turn on again and I also see the ~SHDN pin is pulled low forever (FYI, I set the part to be on latch mode when overcurrent detected)
Thanks