I have the flowing vibration requirement for a board with a PTH08T240WAD on it.
4 to 15 Hz at a 1.52 mm (0.06 in) double amplitude level
16 to 25 Hz at a 1.02 mm (0.04 in) double amplitude level
The data sheet shows the maximum vibration rating for the part as 15G at 20-2000Hz.
Can I assume the part will pass vibration testing because the requirement is lower frequency or is there more to it than that?