This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: State of charge stuck at 0%

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM

Hello,

 I am  newbee using jauge and BqStudio , (bq34Z100EVM and EV2300 , with BqStudio 1.3.86) 
I did the calibration i have configurated cell number (8) , and select the chemistrry.

The final target will be  a pack LiFePo4  u=25.6V ( 8 cells ) capacity 10aHour , but for the 1st tests i am using a variable DC  power supply

The jauge communicate correcltly and seems working, measure voltage and current are correct but State of charge is stuck at 0% ,  MaxError is stuck at 100% ,
all parameters related to capacity does not work

Is there a command to start ?

A last problem , Some Chemistry  can t be programmed , Message is "Chemsitry programming failed Error code=3"  , ex  ID 0456 , (same problem with BqStudio 1.3.97

thanks 

P.CAZENAVE