Other Parts Discussed in Thread: TPS61251
Hi Team,
My customer is using the device and have input from 3.3V LDO (with current limit 200mA) and the same is connected to other loads also. The device turn-on requirement is high as they are having high switching current limit >250mA.
Customer is looking for switching current limit Boost converter IC (Similar to LT8410/LT84101) which can support very light loads.
Required specifications:
I/P Voltage=2-6V
O/P Voltage= >6V
Load= < 5mA
Iq=<50uA
Please help with your inputs and suggestions.
Regards, Shinu Mathew.