Other Parts Discussed in Thread: BQ25895
I just wanted to confirm if this would work or not.
It appears the GPOUT pin is configured by default to be able to disable charging to a charging chip. So does that mean I could just connect it with a pull-up to the nCE pin on the BQ25895 and it will disable charging automatically when it is outside the range of Chg Inhibit Temp Low and Chg Inhibit Temp High ? I would probably just pull this pin up to REG25 pin through a 10k-100k resistor. Then I can just get rid of the thermistor on the BQ25895 and place a 10K resistor in its place?
Thanks