This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: benefit in the application of appliance

Part Number: TPS61165

Hi team,

I have noticed that the one of the target market of the TPS61165 is the appliance:

What's the highlight spec of and the benefit of the TPS61165 in the application of backlight in the appliance? could you please explain the selling point and reason generally?  because after I read the datasheet of TPS61165, i can't found too much special point or highlight.

 

Best Regards,

Wesley Huang

Email: wesley-huang@ti.com

  • Hi Wesley,

         TPS61165 can support 3.3V/5V/12V power rail which can meet almost the power rail requirement;

         Simple PWM/Easy-Scale dimming mode can help customer chose the best dimming mode depends on their requirement;

         Pretty good efficiency and dimming linearity can help to achieve better performance;

    Regards

    Sean