This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: datasheet clarification regarding reset

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQ34Z100

Hello TI,

A two-part question

1) from this old thread:

e2e.ti.com/.../213047

In the paragraph titled "Reset Functions" the data sheet talks about a harware /MRST pin. This pin is not shown in the pin descriptions table. Is this an error or does one of the pins actually have this function.

It appears this remains in the G1 version of the datasheet, yes?

2) If there is no hw-based reset, then is the only way to perform a reset via Host I2C/HDQ control, or will removal of battery power (i.e., deeply discharged battery) also cause reset?

Kind Regards

David McRell