This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQSTUDIO: Unable to import gg.csv file and write to RAM for bq27220

Part Number: BQSTUDIO
Other Parts Discussed in Thread: BQ27220,

I'm having the same issue as detailed in the forums under:  BQSTUDIO: BQ34G100-G1 (Data Flash and Importing GG.CSV file)

Using bqStudio build 1.3.86.  Manually enter all bq27220 fuel gauge settings, create a golden image, and also export the settings to a gg.csv file (which I never open in Excel) for use as a starting point for later refinement. 

When I bring up bqStudio later with fuel gauge EVM attached I "unseal" and "unseal_full_access" the part, then initiate "read_all".  All default ROM values are pulled into bqStudio.  I then import the previously created gg.csv file and all settings appear correct.  However, when I "write_all" bqStudio performs a read of the EVM first and shows all changes between default ROM values and gg.csv file in RED (see image below).  The only way I can apply my settings is to manually enter each field and hit enter twice on the new value (hitting enter once results in default ROM value remaining in place).  After doing this dozens of times I can then "write_all" and then "read_all" to verify my settings are in place. 

Am I missing a step in the import to write value process?  Surely the expectation isn't that golden settings can't be saved for later review/update/write?!