This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22918: TPS22918 VIN and VON power on sequence

Part Number: TPS22918

Hello team,

I have a question about VIN and ON  power on sequence.
I would like the following power on sequence.

  1.   ON pin   0V->3.3V   (VIN=0V)
  2.   VIN pin   0V->3.3V

Is above acceptable of TPS22918?   I am considering to use this sequence although It is not recommended operation range. Is it correct?

If this power on sequence is not acceptable, would you please tell me the recommended other power switch ICs?

Your advise would be so appreciated.

Best Regards,
Akihisa Tamazaki