Other Parts Discussed in Thread: BQ24781
Hi,
Customer is checking PROCHOT behavior with scenario described below.
- NB system runs under a heavy system load with charger adapter connected
- Remove the adapter from the NB and expect to see PROCHOT triggered from ACOK and IDCHG events.
Related set-up and result is described as below.
- Register setting as below. IDCHG threshold is 8192mA
- Resistor value between SRP and SRN is 10mohm
- The waveform at the moment when adapter is removed as below.
- CH1 BQ24781/PROCHOT
- CH2: Battery discharge current
- CH3: BQ24781/ACOK
This PROCHOT is based on ACOK instead of IDCHG based on a separate test previously with IDCHG or ACOK disabled in 0x3DH. From the above test result, the questions are,
- Why we didn't see a PROCHOT triggered from IDCHG event. Based on the IDCHG threshold configured as 8192mA and deglitch time as 100uS, do you have any comment why PROCHOT is not triggered for IDCHG event?
- From ACOK falling edge to PROCHOT driven low it takes 105.6ms. Is it a reasonable delay? I can't find related spec in the datasheet.
Thanks!
Antony