Dear Support,
Our customer wants to use the TPS2561 as high side switch to power two USB 3.0 Ports. I found out that the device protects against reverse current in off-mode.
But now I have two questions:
1. Is it common / recommended to protect USB power switches against reverse current in active mode; speaking of a surge from bus side? If yes: Are there USB high side switches with this functionality or would our customer need a smart high side switch?
2. Is there a meaning after the last letter in the GPN (like TPS20xxC or TPS20xxD) other than the version number?
Thank you in advance and best regards