Can you provide some info on TI PN DCR021205P-U, which is a 2W, 12V to 5V converter.
Occasionally, we get some parts that initially test ok with 5V output but when integrated in the next level assembly, the 5V fails, no output. It would appear as a loading issue but only the DC/DC part is changed and then the system function is established. It may be a transient load that pulls it down but it stays down. The PCB was tested in 3 assemblies prior to being replaced, all with the same results, so it's not likely a problem with the next level assembly. We do have a fair amount of capacitive load, 75uf on board.
Visual inspection of the device & connections looks good. The part is marked with Burr-Brown name and all recent failures have a date code of 88ZE09H. We’ve had about 5 recurrences recently so wondering if anything has changed or maybe these are old parts being used.