Part Number: BQ78350-R2-DEVICE-FW
Hi:
We have an application where two identical battery modules (labelled Pack 1 and Pack 2) are connected in parallel. Each battery pack is running V2.02 R2 device firmware on the BQ78350-R1 and has BQ76930 AFE.
During the discharge cycle, if Pack 1 battery pack terminates discharge earlier than the Pack2, the Pack 2 appears as a low impedance source and causes the discharged Pack1 to trip the ASCD flag. This flag toggles based on its recovery time.
Any way to avoid this in parallel battery connections? or do we have to disable ASCD detection?