This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138: Need help with Full bridge LLC converter design with

Part Number: UCD3138
Other Parts Discussed in Thread: UCC25600

I am planning to design a 3kW ( 540V to 28V) full - bridge converter with UCD3138. 

I designed a full bridge already with UCC25600. However, your engineers pointed out (https://e2e.ti.com/support/power-management/f/196/t/861143) that this IC can't ensure ZVS in both legs.  Attached is the circuit diagram of  my previous prototype. 

My question is do you have any application example of a LLC- converter ( preferably not phase-shifted) for review? I found one evaluation note and there was no description to follow the schematics. Thank you in advance! 

Regards,

Sidd

 5444.TI _ upload.pdf