This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003: LM76003 current limit

Part Number: LM76003


Hello team,

I am considering to use LM76003 as the following condition.
 
   Vin= 24V
   Vout = 12V  max3.5A

I am concerned with LM76003 current limit value of Low side because min value is 3.4A. Is it possible to use LM76003 above condition?




Best Regards.
Akihisa Tamazaki

  • Hi,

    It's low-side current limit and it means as long as you have a valley inductor current below 3.4A, it's OK. When you have a 3.5A load, it mean the average inductor current is 3.5A and if your inductor is not very large, the valley will be less than 3.4A.