This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Type C

Hi,

We want to replace micro USB to USB type C connector. The micro USB connector is used to (charge a single LI-Ion battery) powering the board and not for data communication. Now we need to change the micro USB connector to USB type C connector. 

I was going through web and found that the Type C adapters will not advertise the current or default voltage unless it detects voltage drop across the CC pins (Either CC1 or CC2).  I was looking for a CC controller with inbuilt power path without the power delivery profile. The controller should sink only 5V from the source.

Can you please suggest a suitable part?

Thanks,

Sreekanth