Part Number: TPS61322
Hi team,
My customer is interested in the TPS61322A. Could you support the external parts selection?
Condition
Vin : 3.3V
Vout : 5V
Iout : 200mA(max)
-Output Capacitor
Customer would like to use GRM21BB31H475ME51 or GRM21BR61C226ME44. Could you let me know how much effective capacitance is required for 5V output?
GRM21BB31H475ME51 : Effective capacitance 3.64uF at 5V DC bias
https://psearch.jp.murata.com/capacitor/product/GRM21BB31H475ME51%23.html
GRM21BR61C226ME44. : Effective capacitance 9.883uF at 5V DC bias
https://psearch.jp.murata.com/capacitor/product/GRM21BR61C226ME44%23.html
-Inductor
The Webench recommends 2.2uH for the condition above. On the other hand, the Table.6 in the d/s recommends 4.7uH as well. Which one is better for the condition above? If customer desires lower ripple current, should I recommend 4.7uH?
DFE252012F-2R2M : https://psearch.jp.murata.com/inductor/product/DFE252012F-2R2M%23.html
DFE252012P-4R7M# : https://psearch.en.murata.com/inductor/product/DFE252012P-4R7M%23.html
-External diode(between SW and Vout)
Is the external diode required for the 5V/200mA?
Regards,
Yamaguchi