I need to map some register to the standard SMBus commands at registers 0x3C.
However I cannot find an exhaustive document that tells me how these registers are formatted. For example, I don't if these registers are 8 bits, 16 bits or 32 bits. For "Safety Flags", I assume there is a bit for every event, but I don't know the definition of each bits.
I would also like to know if it's possible to reset the fuse or do a "relearn / initialise" by using the standard SMBus commands at registers 0x3C ? In other words, I'd would like to be able to reset the fuse with a microcontroller.