Other Parts Discussed in Thread: TPS7A24
Dear team, I'm hyunwoo-kim.
There is how to select output capcitor in 14page of datasheet.
there is esr range of capacitor but there is no specific frequency.
As you know , Capactior has various ESR value as frequency so, I think I have to know specific frequency for correct selection output capacitor.
please refer to the below graph, and it is recommened capacitor (TPSC475K035R0600) in TPS763 datasheet.
it has a ESR between 01.ohm and 2.9ohm from 100Hz to 100MHz.
(1) What is the specific frequency to select ESR between 0.3ohm and 10ohm ?
(2) If there is specific frequency or Range , Why do i have to check that frequency ?
Best and Regards,