This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82084: TPS82084SILT no output

Part Number: TPS82084

Hi,

I have used the TPS82084SILT for 5V to 3.3V conversion with 499k as PG pull-up, R2=150k,R1=465K.

Input voltages measured are: EN,VIN are 5V

But output is zero.

The inductor above the IC is measuring 4.35V on one side(near to pin 8) and 4.27 on opposite side.

So is the IC generating output??

Output voltage is always zero even when I kept PG pin as floating

VFB is also zero.

What can be the issue?

How can I troubleshoot?

Regards,

Pavithra.