Hi team,
Can you confirm if TPS7B770x-Q1 can be used for the following use case?
The datasheet specifies current spec 300mA but the internal current limit is min. 340mA. So, is it possible to set the current limit to 325mA?
Rsense : 2kohm (1kohm + 1kohm, divided for 1.8V ADC input)
Rlimit : 750ohm
-. Operating range : 20~300mA
-. Current limit : 325mA
-. Open detection : < 15mA (< 0.06V at ADC input)
-. Short detection : > 307mA (> 1.65V at ADC input)
Thanks,
Sam Lee