This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61161: Inductor Specification Review for the TPS61161

Part Number: TPS61161

Hi Sirs,

Does the inductor P/N FHI2012F-100MT01 (10UH) meet the requirement of the TPS61161 to support 5V Vin, 3 LEDs in series, 20mA peak current?
We can send the datasheet of the  FHI2012F-100MT01 to product line as needed.

Brief specification of the inductor is 10uH +/-10%, Measured at 60mV, 1MHz, 125mA rated current, 0.5ohm DCR, 30MHz SRF.

Thank you and Best regards,

Wayne Chen
02/17/2020