Using the UCD90120, I would like to configure the rails to use the internal temperature sensor on the device to shut down the individual rails due to an overtemp fault. It looks like this is the defualt, but I wanted to confirm.
Also the GPO configuration seems backwards, I’d like to configure an active low ‘FAIL’ signal with multiple failure sources i.e. over temp, NOT power good on 7 rails, over current on 3 rails, and a GPI FAULT input, that’s 12 sources. The fusion SW’s configuration only allows for 4 FAIL sources so I'm a little confused on how to get this done. Also, the AND & OR gates need to changed.
Can you please provide a recommendation on how to set this up in the GUI?