I'm planning on using the TPS3106 for a reset circuit for an FPGA and need to know the output rise/fall times for the output Reset Sense and Reset VDD pins. The FPGA has a requirement on the input that the reset signal needs to have rise/fall times of less than 1us. I'm pulling these reset outputs from the voltage supervisor high with a 10k-Ohm resistor. It didn't seem like there was any specification in the timing diagrams in the datasheet on this.
Thanks