This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: CBn connections when balancing is not used

Part Number: BQ79606A-Q1

Hello, 

Need a bit of help regarding the CBn connections.

Datasheet mentions that if balancing is not used short CBn to CB(n-1).that would mean that if no balancing is used at all, all the CBn pins will be shorted.

However the protector comparators use CBn to measure the voltage and not the VCn pins. if the CBn pins are all shorted then the hardware comparators will not able to work.

What is the correct approach here? I need to use the hardware protectors as this is designed for a safety circuit.

Can CBn be directly connected to VCn pins?

Do i need to use balancing resistors/capacitors for the CBn pins regardless of the fact that i'm not using the balancing function?

Thank you very much in advance