This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22918: PCB Design and Value Selection

Part Number: TPS22918

I have a design using TPS22918. I looked at the datasheet but not fully understand the value selection. 

http://www.ti.com/lit/ds/symlink/tps22918.pdf

That's why I follow the Design Reference on the Datasheet.

My Design: 

Vin = 3.3V

Load Current = 400 mA

Page 17 recommend Cin > Cout 10 times.

That's why I choose Cin= 10uF and CL = 1uF

CT=1000pF

I have Rext =330 Ohm between Vout and QOD (1ms fall time)

And the weird thing here on Page 18 when testing the QOD functionality.

Some tests used Cin = 1uF and CL = 10 uF which opposite with recommendation on Page 17.

Please recommend if those values are good enough for my design.

Thank you very much

  • Hi Trung,

    All of your component values should not cause any problems for your design. Having a 10:1 capacitor ratio is still the recommendation, but because your load is light (400mA) the design would still work with a 1:1 ration if desired (1uF CIN, 1uF COUT). The reason we don't recommend CIN < COUT under all circumstances is just in case the input voltage suddenly drops in your application. If this is the case, then the output may decay slower than the input, and that could cause reverse current from VOUT to VIN.

    In short, no issues with your current setup.

    Thanks,

    Alek Kaknevicius