Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563209: Power consumption at no load condition

Part Number: TPS563209
Other Parts Discussed in Thread: TPS563200

Dear experts,

My customer is testing TPS563209, but find when switching at no load condition, the input current is mA level and too high for them. Is it normal for this device since it seems that no PFM mode?

Or could you help to recommend another pin to pin device for them? They need Vin=10V,  Vo=4.6V, Io=3A, and the power consumption need uA level when operating at load. 

Thanks for your support.