Hi,
I'm looking for a Buck Boost regulator with Dual output. Below are the specification:
Input: 2.7-5/12V (Typically Battery Li-ion operated).
Output: 3.8V@3.5A, 3.3V@250mA.
I couldn't find in product selection.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thank you for posting. This sound more easily to be achieved with a flyback topology, or dual output SEPIC with coupled inductor. The power level and voltage level may need a converter other than a controller. Let me forward this to our converter IC experts.
Thanks,
Youhao Xi, Applications Engineering
Hi
if I understand correctly, the input power is lithium-ion battery or 12V, here my suggestion
a boost converter TPS61089 to 6V output, then connect the 12V input to the output of the boost. the 12V is higher priority to power the downstream loading.
from 6V~12V input to 3.8V output, we need a 3.5A buck converter to generate 3.8V. the 3.5V output can be an LDO from 3.8V to 3.5V.
then the solution is simpler. you can use a low voltage buck-boost http://www.ti.com/lit/ds/symlink/tps63810.pdf for 3.8V, then a LDO to 250mA.
Hi
I would suggest to pull high through resistor, but you can't change the VOUT to 3.8V without the I2C.
what is 3.8V 2A is used for in this application?
Hi Lakshminarayana,
As Jasper suggested, the TPS63802 can be used, with somewhat loosened requirements for the minimum input voltage.
Alternatively, you could consider the TPS63806 which can support up to 3 A at Vout = 3.6 V, Vin = 2.8 V. The TPS63806 is similar to the TPS63802, but with increased current limit and it comes in chip-scale package.
Do you expect continuous maximum output current of 2 A, or just a pulse?
Best regards,
Milos
Hi Lakshminarayana,
Please take a look at the TPS63802 datasheet, Figure 14, and the TPS63806 datasheet, Figure 17, for maximum output currents at Vout = 3.6 V. The TPS63802 has higher output current capabilities than the TPS63020. The TPS63020 would not be able to support your load.
The TPS63806 should be able to handle your load, but is comes in chip-scale package which is not as easy to handle as the DFN package for the TPS63802. In any case I can test your load on both devices. Could you please tell me what is the length of your 2-A pulse?
Best regards,
Milos
Hi Milos,
Thank you.
" Could you please tell me what is the length of your 2-A pulse? " typically for few microseconds(us) - (cellular 2G).
One query on TPS63802, In the pin description, for the Mode pin - set Low for PFM(power saving mode-Highest efficiency for lower current) and High for PWM Mode.
But in the Figure 17-Efficiency versus Output Current graph, Mode is HIGH and PFM? and highest efficiency?
Thanks
Hi Lakshminarayana,
For power-save mode the MODE pin needs to be set LOW. The pin description table is correct, the description in the images is not and will be corrected in the next datasheet revision, sorry for this.
The length of a high current pulse can be limited by the thermal management. Therefore even though Figure 14 from the datasheet shows that the TPS63802 can support 2.5 A at Vin = 3 V, the current capability can be reduced if the device overheats. But if the pulse length is below ms, there should be no problems.
Best regards,
Milos
Hi Lakshminarayana,
Of course. Please make sure you are following the guidelines from the datasheet.
Best regards,
Milos