Is there a way to exit the ship mode when the 14 second timer is enabled but the CPU cant perform a i2c access. This is a development issue where we are trying to flash a unit that is in ship mode. For example can we change io state to disable the 14s timer? Do we need to remove the battery?