Other Parts Discussed in Thread: BQ78350, BQSTUDIO, EV2400
Hi.
We use the BQ78350 with the BQ7693000DBT for a battery of 36 V 10400 mAh for an ebike.
Using the e-bike, in some moment the display displayed a state of charge near 50% but suddenly displayed 0%.
We could not have acces directly to the fuel gauge but the MCU that communicates with the fuel gauge give us the information that the TDA alarm, RCA alarm and RTA was active and with a state of charge of 0% but still discharging.
The voltage measure indicated 36.54 V
So, what could be the cause that the fuel gauge will suddenly send a percentage of 0% and without DSG protections?