Team,
I wanted to clarify a few questions in regards to the TLC59116 IC:
- This part can be programmed to perform the blinking feature as long as the blink frequency is between 24 Hz and 10.73 seconds
- If utilizing the LED all call feature to program all drivers at once does the register auto increment feature still work?
- If a device is programmed to acknowledge the LED all call address will it still acknowledge it’s individual i2c address, or must the all call be disabled?