Hi ,
regarding the low side feedback resistor for the positive output (8.2.2.2 on the datasheet), the description says the resistor R2 should not be no less than 50kohm.
Is this because there is a risk of instability when the current is too high?
Or is it supposed to the the reverse and having too high of a low side resistor could increase susceptibility to noise?
Thank you much!
Regards,
Alberto