This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5163: About selection of Cout

Part Number: LM5163

Tool/software: WEBENCH® Design Tools

Hi TI-team

I calculated the following condition using WEBENCH.

Vinmin=30V, Vinmax=90, Vout=15V Iout=0.5A.

In additon, I optimized with Small Footprint Design.

Then Cout is 3.3μF.

The data sheet recommends 22μF in consideration of the voltage coefficient, but isn't it considered in WEBENCH ?

Should I choose a capacitance that becomes 3.3μF when Vout = 15V ?

 

Best Regards,

Koji Hayashi