This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3850: Comparator Accuracy Histogram Data

Part Number: TPS3850


I am monitoring a 3V3 rail which requires particularly tight windowed monitoring.  Using the worscase accuracy figures from the datasheet on the comparator accuracy of 0.8% results in the thresholds being 0.009V outside my requirement.

Looking at the datasheet section 6.7 states that measured over 41,111 units the measured accuracy is within 0.2% while the temperature drift adds a further 0.2%.

What guarantees can you give that the devices will actually operate with a comparator accuracy of say 0.45%. Are there process controls that keep the devices behaving as per the section 6.7 sample.

Best Regards,


Dan Minors

GE Aviation