This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2592HV: Support to check for a new IC with the desired input and output range.

Part Number: LM2592HV


Good afternoon all,

I am writing this query to know mainly about following things:

1. The step down DC DC converter LM2592HV having the I/P range 4.5 to 60V and two fixed and adjustable O/P versions. I just wanted to know, whether in the datasheet Adjustable O/P versions means can we have the O/P values ranging from 0 to 24V dynamically? .Our requirement is such, we want 0 to 24 voltage which is one time programmable , and works according to the PWM signal given as the input.

2. Telling the same, can you please let me know if there is a IC (step down DC DC converter) which has input range 24 to 60V and can take PWM signal as input. And the output voltage having the range 0 to 24V which is dynamically programmable and varies according to the input PWM signal and should give the output current max 2A.

Please do help me in finding one IC.

Thank you in advance

Ramya L