This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Learning Issue

Part Number: BQ34Z100-G1

Hello

Regarding learning problem I have

I can’t get an accurate FCC after learning.

The battery is 7s6p with 17.4AH capacity at the voltage range It should works- 29.4V- 19.6V

After learning I got FCC=16.78AH. the actual measured capacity= 17.4AH

Enclosed log file of the Learning Discharge and gg file I programed before the learning.

Please note that at the end of discharge the FCC=17.6AH after few min it updates to 17.8AH and after about 2 hours it goes to 16.78AH.

Also note that the original Qmax Cell 0 is 1800 and after charging it jumps to 1900.

Best Regards

initial.gg.csvlearning_cycle_2_discharge.log