Hi
I'm selecting power regulators for my design. Now I'm checking for switching regulator with
1. -6V @ at least 1A output from 5V input
2. 30V @ at least 1A output from 5V input
Regards
Nidhi P Shetty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Thank you so much for your support.
I've changed my architecture in such a way that, I need around 10mA current output from both 30V and -6V regulators. Recommended is charged pump regulator. Suggest the best option for the same.
Regards
Nidhi P Shetty
Hi Nidhi,
the 30V output should be a boost such as TPS61170, as charge pump can't support this high voltage.
the -6V could be charge pump, but the typical output would be -5V if the input is 5V.