Hi,
Solenoid is rated: 12 VDC, 60.2 Ohm, 2.5W, 199mA
Application is in high security door locks, which are powered from either 12V or 24V depending on existing access control systems. Original design was to drive solenoid directly for 12V installations and use a simple dropping (i.e. current limiting) resistor for 24V applications. However testing has shown that at 12V solenoid does not provide enough pull force to reliably retract plunger. Reliable actuation can be achieved with 13-15V. Per solenoid manufacturer solenoid can be operated continuously at up to 15V.
So I am looking for a simple, small footprint DC-DC converter which will accept either a 12 or 24V input and produce a fixed 13-15V output at about .3A max.
I have done some testing with an inexpensive "DC-DC Boost Buck adjustable step up down Converter Module" which are available all over EBay, Amazon, etc... These are based on an XL6009 regulator from XLSEMI configured as what to me looks like a SEPIC topology. This module seems to work ok, and I have found a schematic as well as the datasheet for the XL6009. However I do not see much info regarding the XLSEMI brand, nor does it appear to be available through typical distribution channels.
Module ref. link below: "DC-DC 1.5V - 35V Adjustable Boost Buck Step Up / Down XL6009 Converter Module"
https://www.ebay.com/itm/DC-DC-1-5V-35V-Adjustable-Boost-Buck-Step-Up-Down-XL6009-Converter-Module-/192019886845
Note only load is the solenoid plus a couple status LED's. No other active electronics where noise or ripple would be a concern.
Estimated available PCB space is approx. 2.25 sq. in.
Can you recommend any TI parts or designs to consider as a solution for this requirement?
Any advise you can provide greatly appreciated.
Thanks,
Henry (Hank) Zagara
Z-TECH EMS (Electronics Manufacturing Support)
3 Manlon Terrace
Cheektowaga, NY 14225
716-465-6990
hank.ztech@roadrunner.com