Other Parts Discussed in Thread: TMS320VC5501
Hi Sir,
I have several issues about TPS73HD301 by our customer. They use this part as voltage regulator and supervisor for TMS320VC5501. But they found the RESET function sustained active when system power on.
1. The output voltage of adjustable regulator is 1.26V, but in terms of the description from datasheet the adjustable output voltage below 1.9V the RESET function become unusable. Therefore, could you help me to confirm TPS73HD301 can work well under Vout1 = 1.26V condition? Or is this application totally can not apply?
2. According to their testing, they found RESET function sustained active when the temperature decrease which cause output capacitor ESR increase, so they change output capacitor from electrolytic type (47uF/10V, ESR = 1.35 Ohm) to ceramic type (47uF/10V, ESR = 20m Ohm), then the RESET was not active. Hence, they want to confirm, is the RESET function error is due to the output capacitor ESR and change to ceramic capacitor will fix this issue? Does this change affect the circuit stability?
3. What is Trip-threshold voltage? Is it the reference voltage for RESET gate drive or has other meaning?
4. Do you have any reference design for this part?
Best Regards,
Hughie Lu