This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21225A: Need help getting the UCC21225A PSpice model and schematic working at 1MHz vs 100kHz.

Part Number: UCC21225A


Need help getting the UCC21225A PSpice model and schematic working at 1MHz vs 100kHz.

  • Figured it out.  Just need to tweak the DT resistor.

  • Hi, Joseph,

    Thanks for letting us know!

    By the way, if you're using a large value DT resistor, please heed this advice in the data sheet:

    "It should be noted that the UCC21225A dead time setting is decided by the DT pin configuration (See Programmable Dead Time (DT) Pin), and it cannot automatically fine-tune the dead time based on system conditions. It is recommended to parallel a ceramic capacitor, 2.2-nF or above, close to DT pin to achieve better noise immunity and dead time matching.

    Let us know if you have any other questions.