This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27531-G1: Parameters for replacing the battery

Part Number: BQ27531-G1
Other Parts Discussed in Thread: BQ24193, BQSTUDIO
For a removable battery pack, bq27531-g1 / bq24193 is mounted on the system side.
There is only one kind of battery pack, but I want to calculate the remaining amount immediately when a spare battery is installed.
I want to save the bq27531-g1 parameter in the EEPROM inside the battery pack and read and write it when using it.
Which parameters should be saved?