Hi Team,
Could you kindly advise on the below figure13, 14 ?
For instance, if the input condition was figure13, would the output voltage would regulated voltage plus AC coupled voltage ?
And if fast transient was inputted, will the output voltage be over than regulated voltage ?
(If TLV76750 is used, will output voltage be more than 5V at fast transient input.)
Thank you and best regards,
Michiaki