This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS756: Mounting Tab

Part Number: TPS756


Is central pin electrically connected to the mounting tab in all packages (DDPAK and TO-220)?

  • Hi Hussien, 

    The central pin is almost always connected to the mounting tab and they both need to be connected to the ground plane. I don't see a reason this device should be otherwise. I opened the wire bonding diagram for the two packages, and they are connected. 

    Regards, 

    Jason Song